What is a living hinge and its applications?

Worker about to install a conventional hinge on an industrial application

Living hinges are durable and can be used in a wide number of applications, so it’s worth understanding a little more about them. In this article we cover: 

What is a living hinge?
Types of living hinge design
Manufacturing methods of living hinges
Living hinge vs conventional hinge: which to use?
Limitations of living hinges
What applications can a living hinge be used for?

What is a living hinge?

Living hinges are made of a thin, flexible section of (usually) plastic that’s used to connect two rigid sections on an item or appliance.

Often, the two sections and the living hinge itself are fashioned from one continuous, moulded piece of plastic. But, you can also purchase individual living hinges that can be attached to the two sections you’re attempting to connect using mechanical fixings.

Plastic continuous hinge

Living hinge names and types

It’s worth noting that living hinges don’t always go by that name.

They’re sometimes called plastic continuous hinges or piano hinges, although you’ll find the exact definition of each may vary depending on where you look and what they’re made of.

Looking for dimensions?

Take a look at Essentra’s continuous hinge size chart for a list of all our continuous hinge sizes.

What's the difference between a living hinge and a conventional hinge?

A conventional hinge (or traditional hinge) typically needs some kind of central pin or rod in order for it to be able to turn, as seen in the examples here:

Continuous hinge technical drawing

A living hinge, on the other hand, is fashioned from a single piece of material. Its design simplicity is shown here, in Essentra Component’s continuous hinge

Woman prototyping on a 3D printer

Types of living hinge design

There are four main kinds of living hinge designs, each with its own advantages:

The Four Primary Living Hinge Design Types
Flat / straight hinge By far the most widely used living hinge. It consists of two straight strips with a narrow, flexible hinge section.
Double hinge Comprises two straight living hinges separated by a narrow landing strip. Double hinges are useful for applications where space is needed between the two connected sections, or the hinge needs to rotate 360˚ instead of 180˚.
Butterfly hinge Commonly used on dispensing caps, butterfly living hinges are what we often refer to as flip-top caps. Once the hinge is opened or closed past a certain angle, the hinge will complete the rotation then stay in the full open/closed position.
Bi-stable hinge
 
Basically a butterfly hinge with added “oomph.” Where the butterfly living hinge has a single hinge section, the bi-stable living hinge has three. Like the butterfly hinge, the bi-stable hinge will snap open or closed once it reaches a certain angle; the added hinge sections result in a stronger action and added stability in both end positions.

 

Manufacturing methods of living hinges

If it’s a custom living hinge you need, it’s worth knowing about the various manufacturing methods.

3D printing

Until recently, the best way to produce a prototype living hinge was through CAD and CNC machining.

But 3D printing has grown enormously in prototype manufacturing: it’s quick, cost-effective and, often, entirely automated. 3D printing is best suited to creating single prototypes for demonstration purposes, as printed hinges don’t have the same durability as those manufactured in other ways.

CNC Laser cutting industrial technology

CNC machining

When you think of CNC machined hinges, your mind probably jumps straight to something like heavy duty steel hinges rather than plastic.

But there’s still a lot to be said for CNC machined plastic — as long as you work with a company with skilled machinists, you can get great results. CNC machining is perfect for producing prototype and test batches of products with plastic living hinges.

It’s quicker and far more cost-effective than moulding, particularly if it transpires that the design needs to be changed.

For prototype batches of around 100 units or more, you’ll want to consider paying for custom tooling, and going down the moulding route.

Injection moulding

If you’ve perfected the design of your living hinge, and you’re ready to mass produce, it’s time to move on to injection moulding.

Once you’ve made the initial lay-out for the design and manufacture of bespoke tooling, injection moulding is by far the fastest and cheapest method of producing items with living hinges.

Laser cutting

Not your typical living hinge, but still worth a mention due to its growing popularity. You can use a laser cutter to create living hinges in thicker sheet material such as MDF.

This kind of living hinge is still weighted towards aesthetics rather than durability and is often used for luxury commercial items like notebook covers, folders and laptop cases.

Extrusion

Extrusion is used when creating plastic continuous hinges that are designed to be attached to other items, so it’s far more relevant to hinge manufacturers than product engineers.

Like injection moulding, extrusion uses heat to mould an item into a particular shape – In this case, a cross section. The heated plastic is forced through a die and, when it cools, it solidifies.

Production line with industrial doors ready for installation

Living hinge vs conventional hinge: which to use?

It can be hard to know when to use a particular kind of hinge, so we’ve broken down the main characteristics of living hinges here. The primary advantages include:

Applicability

Living hinges are compact, simple and versatile, which makes them suitable for a vast range of applications, both commercial and industrial, such as light-duty HVAC components.

Durability

With their unibody design, moulded living hinges place high on the durability scale. There’s nothing to fiddle with and they operate with zero friction, so they tend not to suffer from the same wear and tear that conventional hinges endure, even after hundreds of thousands – or millions – of cycles. This makes them a popular clip-close solution for things like enclosure door latches.

Assuming they’re manufactured correctly, and not damaged or subjected to unnatural conditions, living hinges can be expected to last the whole lifespan of the item they’re part of.

Cost-effectiveness

Made from a single part, living hinges are far less expensive to produce en masse than conventional hinges, which require a variety of tooling, multiple components and manual assembly.

If you’re opting for a custom living hinge, keep this in mind. While the initial outlay for moulds and bespoke tooling can be quite expensive, the time and money recouped during mass production easily offsets this cost.

Chemical resistance

Living hinges are typically made from plastic, which won’t rust like conventional metal hinges. Because plastic living hinges won’t corrode like stainless steel hinges, they’re often favoured for use on, for example, an outdoor utility cabinet, outdoor electrical enclosure or an outdoor telecom equipment cabinet.

Flexibility

Living hinges offer brilliant flexibility around their point of rotation, typically offering more than 180˚ in standard straight living hinges.

Living hinge design can be tailored to offer 360˚ rotation, or to limit rotation at a particular angle if needed.

This added flexibility is useful in applications where the lid needs to rotate by 180˚+ and move completely out of the way, such as electrical enclosure door hinges and data centre server cabinets, where unrestricted access is needed.

Length

Long plastic continuous hinges can be used to provide uniformly distributed support and stability along the rotating edge of your product, reducing the weight and stress placed on the both the connected sections and the hinge during each cycle.

This added stability is well suited to compact, wall-mounted plastic cabinets, and gives living hinges an edge over different types of cabinet hinges.

Outdoor cabinet with concealed hinges

Limitations of living hinges

Like any kind of hinge, living hinges have their weak points. You’ll want to consider conventional hinges if you’re prioritising any of the following characteristics in your design:

Strength

Living hinges aren’t favoured for their strength, nor are they suited to applications where two (or more) weighty sections are being connected.

So while they’re suited to some industrial applications, they’re just not strong enough for others. They’d work fine as part of a heavy duty door latch, for example, but they’d never match up to the usual heavy door hinge types. With their highly flexible middle section, living hinges have very limited load-bearing ability and can easily be damaged by excessive force, particularly if it’s applied unevenly to the hinge.

Thermal stability

Plastic has a relatively low melting point, which means that your typical living hinge is completely unsuited to applications in which it’ll be subjected to extreme heat.

Likewise, polymers tend to become brittle and easily breakable when exposed to extremely low temperatures. It’s best to use living hinges only for items that will be used in moderate temperature environments.

Lack of material choice

Living hinges are almost always manufactured from plastic, usually polypropylene PP or polyethylene PE. Learn more about the differences between these two plastics in our guide, PP vs PE

And while you can use additives to enhance or reduce certain characteristics inherent within the polymer, you’re still limited as to how much you can alter its make-up before you risk compromising the effectiveness of the hinge.

What applications can a living hinge be used for?

Living hinges are everywhere you look in the consumer goods market. They’re flexible, resilient, impervious to moisture, and cheap to mass produce, which makes them the perfect solution for:

Consumer applications Industrial applications
Bottle caps for food, drink and personal hygiene products Outdoor enclosure door hinges
Cosmetic compacts Weatherproof outdoor cabinets
‘Click-lock’ closures on food storage tubs Different types of electrical junction boxes
Tool boxes Hinged parts of an HVAC system

 

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download. You can also request free samples (some exclusions apply) to ensure the product you’ve chosen is exactly what you need. 

If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.

Request your samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.