How to prevent galling on stainless steel bolts

Stack of metal fasteners and washers

What is Galling and what causes it to happen?

Galling is one the most common problems when tightening fasteners. Also known as cold welding, galling results in damaged threads, broken fasteners, weakened joints and seized bolts. Essentially, to define galling - it's a form of severe adhesive wear.

Galling happens during installation to fasteners made of alloys such as stainless steel, aluminium and titanium. While the fastener is being tightened, pressure builds between the thread surfaces and breaks down the protective oxide coatings. Without the oxide coating, the thread’s metal high points are exposed to each other. This, in turn, creates friction, which causes heat that seizes the metal. These can be the reasons of galling on stainless steel bolts and other materials. 

What to do when galling happens and how to avoid it:

If the galling is minor, slight damage may occur to the thread surface. In that case, the installer may be able to remove the fastener. On the other end, severe cases of galling can weld the nut and bolt together and there is no way to remove the fastener. If the fastener is tightened once galling begins, the fastener may even be twisted off or see its threads stripped.

The factors that can impact galling are:

  • Design
  • Applied load
  • Contact area and degree of movement
  • Lubrication
  • Surface finish and hardness

How do you minimise the risks of galling?

• Think about your material

Highly ductile materials, or materials which possess low work-hardening rates, are often prone to galling. For instance, austenitic stainless steels have a tendency to gall under certain conditions, though you can minimise this risk by using a hard nut of duplex stainless steel. Brass and bronze are frequently used for bearings, bushings and other sliding applications due to their tendency to resist galling.

• Choose coarse threads

Opt for coarse threads with a 2A-2B fit by the Unified Thread Standards. Coarse versus fine threads give you a larger thread allowance and are more tolerant to abuse during handling.

• How hard?

Make sure your nut and bolt have a hardness difference of at least 50 Brinell. This is because the different alloys harden at different rates, lessening the chance of galling.

• Think about design tolerances

The mechanical fit should be correct – tight enough to prevent vibration and wear, but with sufficient clearance to prevent galling. Keep the contact load on the components that slide to a minimum, and the contact area, maximised.

• Keep it clean

Surfaces should be smooth and clean from dirt and dust that can settle between mating surfaces.

• Specify the threading method

Design engineers who specify threaded parts are missing a trick when they fail to also specify the machining methods, leaving it to the machine shop to decide. But deciding on the machining method can prevent premature failure, improve strength and even cut production costs.

There are two types of machining methods: thread cutting and thread rolling. Thread cutting uses sharpened tools to remove material to form threads, which are rough with minute chips. These chips can cause galling.

If your application requires consistent thread geometry or will be assembled and disassembled often, then specify thread rolling. This is a cold-working process. Steel dies force the material outward into the shape of threads, providing smooth finishes. Thread rolling also provides superior tensile and fatigue strength.

• Smooth rough edges

It’s worth noting that highly polished or rough surfaces tend to gall more. Wipe a rag over the thread surface. If it snags, it will most likely gall when assembled. Electropolishing will smooth any rough edges on your surface finish and reduce the possibility of galling.

• Use lubricant

To reduce friction, choose an appropriate lubricant. Lubrication is required even if the joint is intended to be permanent. However, if your application involves food, you’ll have to avoid many lubricants, so beware.

• Slow down

Heat is a significant factor in galling. To lessen the heat, minimise the friction. You can do this simply by lowering the wrench speed during installation or removal.

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download for free. You can also request free samples to ensure the solutions you’ve chosen are exactly what you need. If you’re not quite sure which product will work best for your application, our experts are always happy to advise you.

Request your free samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.