Guide to choosing the right cable clamp | Essentra Components US

Guide to choosing the right cable clamp

Man screwing a cable clamp onto a consumer appliance

In another guide, we discussed using cable tie mounts for securing wire and cable bundles. In this guide, we'll discuss another option for mounting cables on the panel boards of various types of enclosures, such as a data centre server cabinet or an outdoor telecom equipment cabinet.

Using a cable clamp has some distinct advantages over cable mounts. For example, if you need to move, adjust, or add to the bundle while using a zip tie mount, you must cut the tie.

Many cable clamps can be opened to allow for easy adjustments. While ties can still be used for bundling, you'll often find you need fewer of them when bundles are secured with clamps.

In many instances, making up a new enclosure is faster when using cable clamps. Once the wire cable clamp installation is complete — guided by a good set of layout diagrams — cable and wire installation consists of routing the cables and conductors and snapping them into place.

Server room with lots of disordered wiring  around data centre server cabinets

As with cable tie mounts, you have a good selection of mounting options:

  • Adhesive cable clamp mounts
  • Fir tree push on mounts
  • Arrowhead push on mounts
  • Screw or rivet on mounts

So while the mounting options are similar, there are two major differences between a cable tie mount and a wire cable clamp: ease of cable installation and replacement, and the ability to set wire bundles at varying heights.

Adjustable cable clamps accommodate several diameters of cable or wire bundle with one size clamp or clip. One example is an adhesive backed cable holder that uses a ratcheting feature to allow several bundle sizes to be securely clamped. Additionally, the clamp can be reopened without damaging it. This allows the technician to trace wiring problems or reroute cable when necessary.

The ability to reopen a cable clamp is one of the main and most valuable features. It can be accomplished in various ways. Hook & loop clamps are quite versatile and their adhesive mount allows for quick, simple installation of the cable clamp. Network cable enclosure and support systems cabinets often use these clamps, as do rack enclosure cabinets. A hook & loop clamp can be either top or side opening to match the enclosure design.

Truck on production line showing wire cable clamp installation

 

Wiring harness cable clamps with a screw mount are often used to aid in automotive wiring protection when wires are bundled using a sleeve, heat shrink tubing, or wire wrap. They flex at the opening to allow easy installation or removal of wire bundles.

Some cable clamps have a hinged locking clamp that allows easy opening and secure clamping of various bundles. The fir tree mounted locking cable clamp is easy to install on various thicknesses of panel boards.

For safeguarding power wiring – such as motor leads – in outdoor weatherproof electrical enclosures used in HVAC systems, an adhesive cable mount for 3-wire leads help keep power wires secure and untangled.

One thing that's difficult for cable ties to do effectively is secure ribbon cables without bending them. For inside a computer chassis, wall mount rack enclosure server cabinet applications, and similar enclosures, a flat cable clamp works best. The ribbon cable is slid into the clamp from the side and is held in place by the tension provided by the clamps design. The clamp is normally an adhesive backed cable holder.

For efficient wiring protection – whether you're routing cables, cable bundles, or specialty cables like fiber optics – cable clamps provide many options. To ensure a proper fit and wire cable clamp installation, be sure to consult the clamp manufacturer's instructions.

When installing specialty cables – particularly with delicate data cables – make sure you're using the correct clamp for the cables involved. For example, follow fiber optic cable installation guidelines to make sure the cables are not damaged by using an improper cable bend radius.

Closeup of coloured electric cables

Choosing the correct cable clamp will ensure a clean, easy-to-manage cable installation. Here are some simple guidelines to get you started.

Standoff clamp

Cables raised off the panel-board surface

Standoff clamp

 

 

Adjustable adhesive diameter clamp

Ability to adjust for cabling changes

Adjustable adhesive diameter clamp

 

Adhesive backed clamps, D style

Quick and simple installation on flat, dry surfaces

Adhesive backed clamps, D style

 

Round cable clamps, plug in

Push-in-place installation for pre-drilled or non-predrilled applications

Round cable clamps, plug in

 

Multi-cable clamps, screw mount cable grips

Run multiple cables or cable bundles in parallel

Multi-cable clamps, screw mount cable grips

 

Flat cable clamp, adhesive mount, tension

Run ribbon cables for computers and other applications

Flat cable clamp, adhesive mount, tension

 

Steel cable clamps with rubber cushion

Hose protection, vibration absorption and electrical insulation

Steel cable clamps with rubber cushion

 

U-clamp, screw mount

Prevent cables from shifting and, or, tipping

U-clamp, screw mount

 

Strain relief clamp

Add support for strain relief

Strain relief clamp

 

Half U snap-in cable clamps

Route wire bundles in limited space

Half U snap-in cable clamps

 

The success of your project often depends on the proper routing of cables, cable bundles, and wiring. For the most versatile, professionally designed panel board or enclosure, choose the proper cable clamps to facilitate your application.

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download. You can also request free samples to make sure you’ve chosen exactly what you need. If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.

Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.com or speak to one of our experts for further information on the ideal solution for your application 800-847-0486.