304 vs. 430 stainless steel: what’s the difference?

Stainless steel tubing

What is 304 stainless steel?

Stainless steel grade 304 belongs to the austenitic stainless steels. It contains a minimum of 18% chromium and 8% – 10.5% nickel with a maximum of 0.08% carbon. Find out more about austenitic stainless steels in our guide,What are the differences between carbon steel and stainless steel?

Chromium is the key element here – and it’s where stainless steel’s superior corrosion resistance comes from. The chromium forms a passive oxide layer on the surface of the steel, protecting it from rust and corrosion. The higher the chromium content, the greater the resistance to corrosion. Chromium also enhances the steel’s toughness and ductility, making it easy to work with. It’s also why 304 stainless steel stands up to high temperatures.

Nickel increases its resistance to corrosion, especially against acidic environments. The material's toughness and ductility is also helped by nickel, making it easier to form and fabricate. Carbon is added to improve the steel’s strength and hardness. However, if the carbon content is too high, it reduces the material's resistance to corrosion and makes it more difficult to weld.

304 stainless steel also contains small amounts of manganese, silicon, and sometimes molybdenum. These elements all contribute to the material's strength, formability, and weldability.

304 stainless steel is non-magnetic, which makes it useful in applications where magnetism is undesirable. This comes down to its austenitic microstructure, which is a face-centred cubic (FCC) crystal structure. The atoms in the lattice structure are symmetrically arranged, and their magnetic moments cancel each other out.

You can learn more about the different grades in our guide, Understanding stainless-steel grades.

What is 304 stainless steel used for?

With excellent corrosion resistance, this metal is commonly used in these applications:

Industry Typical applications Why
Food processing equipment Tanks, pipes and containers Resistance to corrosion, easy to clean
Consumer appliances Sinks, refrigerators, dishwashers Durability, resistance to corrosion, aesthetic appeal
Automotive Exhaust systems, trim and grilles Resistance to corrosion, aesthetic appeal
Medical equipment Medical devices such as surgical instruments, dental instruments and implants Biocompatibility, resistance to corrosion and withstands high-temperature cleaning processes
Chemical processing equipment Reactors, tanks and pipelines Resistance to corrosion, stands up to a range of chemicals
Aerospace components Aircraft structures, engines High strength-to-weight ratio, resistance to corrosion, thermal stability

304 stainless steel is also used in small components. Examples include:

Worm-drive hose clamp

Worm-drive hose clamp

  • Band, housing and screw are 304
T-handle

T-handle

  • 316 base material and 304 for smaller pieces. 

 

Fan filter

Fan filter

  • Mesh is 304

Properties of 304 stainless steel

The characteristics of 304 stainless steel – as with any material – are a result of its properties. Let’s take a closer look:

Properties of 304 stainless steel
Stainless steel medical equipment

What is 430 stainless steel?

Explaining this stainless steel grade is easier when we consider 304 vs. 430 stainless steel differences. First, 430 belongs to the ferritic stainless steel grades with 17% chromium. Grade 304 has slightly higher chromium content with a minimum of 18%.

Grade 430 also lacks nickel. This makes 430 stainless steel not as strong for corrosion and chemical resistance in harsh environments when compared to 304 stainless steel. Mind you, grade 430 still has very good corrosion resistance – it’s just not quite as high as 304 stainless steel. Also, be aware that the absence of nickel can make 430 stainless steel vulnerable to cracks during pressing.

430 stainless steel does have good thermal conductivity, which helps in applications where heat dissipation is important. It also has slightly higher heat resistance compared to 304 stainless steel.

Magnetic catches

Unlike 304 stainless steel, 430 is magnetic – hence, why it’s ideal for magnetic catches, as seen here. Like 304, 430 stainless steel also has good formability. However, ultimately 304 stainless steel has more versatility in its applications, hence why it's the most widely used of all stainless steels.

What is 430 stainless steel used for?

430 stainless steel costs far less than 304 stainless steel, which comes down to grade 430’s lack of nickel. While the price of metals constantly fluctuates, it’s not unusual to see grade 430 cost anywhere between 55% and 75% of 304 stainless steel.

304 vs. 430 stainless steel uses have some overlap. Common applications for 430 stainless steel include the following:  

Industry Typical application Why
Automotive Mufflers, trim Corrosion resistance properties
Aircraft Compressor blades Corrosion resistance properties
Energy/power generation Turbine engines Corrosion resistant, maintains strength in heat
Consumer appliances Refrigerator cabinet panels, range hoods, dishwasher linings Cost effectiveness, easy to clean
HVACs Heat exchangers, furnace parts Thermal conductivity, Resistance to corrosion
Components Fasteners/screws, Worm-drive hose clamp Ease of fabrication, Resistance to corrosion

 

Properties of 430 stainless steel

304 vs. 430 stainless steel properties, or rather, 304 vs. 430 appearance: Both have aesthetic appeal. Grade 430 has excellent finish properties, and coupled with its costs, it explains why it’s also used for decorative purposes, such as in elements of architecture and jewellery

Properties of 430 stainless steel
Stainless steel turbine engine

304 vs. 430 stainless steel: a comparison

It helps to see the composition of these stainless steel. As you can see, they’re similar in many ways, but the lack of nickel in grade 430 is their main difference.

Element 304 stainless steel % 430 stainless steel %
Carbon 0.07 0.08
Chromium 18.0 – 19.5 16 – 18
Nickel 8.0 – 10.5 -
Silicon 1.00 1.00
Manganese 2.00 1.00
Phosphorous 0.045 0.045
Sulphur 0.015 0.015
Nitrogen 0.10 -

 

304 vs. 430 stainless steel strength

Grade 430 contains slightly more carbon, which means it should be stronger than 304. That said, the nickel in grade 304 contributes to its strength. Here’s how they’re mechanical properties compare – note, the ultimate tensile and tensile yield strengths measure the materials’ resilience to tensile (pulling) forces. The yield strength reflects the maximum stress before the material will deform permanently. The ultimate tensile strength describes maximum stress before fracture.
 
To understand the Rockwell B hardness test, see our guide, What’s shore hardness and why should you care?

Properties 304 stainless steel 430 stainless steel
Ultimate Tensile Strength 505 MPa 517 MPa
Tensile Yield Strength 215 MPa 345 MPa
Hardness (Rockwell B) 70 85
Elongation at Break 70% 25%

 

304 vs. 430 stainless steel differences

In summary, these are the primary characteristics of both steels:

Characteristics 304 stainless steel 430 stainless steel
Corrosion resistance Excellent Very high
Magnetic properties  No Yes
Weldability High Limited
Hardens during cold forming Yes No
Formability Very good Good
Machinability (annealed) Fair Good
Resistance to elevated temperatures High High
Maximum intermittent service temperature 850°C 850°C

 

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download. You can also request free samples to make sure you’ve chosen the right product for what you need. If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.

Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.