Low, medium, and high-carbon steel: everything you need to know

Carbon steel in mechanical application

Different types of steel cater for different purposes with a vary of specific features. In this article, we will focus on different types of carbon steel and explore the uses, types, grades and properties of each.

Explore by type:

  • Low carbon steel
  • Medium carbon steel
  • High carbon steel

Looking for something specific?

If you want to learn more about the differences between iron and steel, you can read our guide: What is the difference between iron and steel?

What is low-carbon steel?

Low-carbon steel, also known as mild steel, has a comparatively low radio of carbon to iron compared to other steel types. Typically, its carbon content is within the range of 0.05% and 0.32% by weight. This gives low-carbon steel low strength while making it more malleable and ductile compared to high-carbon steel.

One of the major benefits of mild steel is its cost-effectiveness. As it requires less carbon and other alloying elements, it’s normally less expensive than other types of steel. Moreover, it’s more readily available and simpler to work with than higher-carbon steels, which makes it a popular choice for a wide range of applications.

What are the uses of low-carbon steel?

Despite its low strength compared to other steel types, low-carbon steel is still strong enough for use in structural applications. It’s also used for machinery parts, as it helps to reduce machining costs. It’s easy to shape, which speeds up production times and reduces the cost of machining compared to other materials, such as aluminium.

Mild steel is also used in industrial small components, ranging from fasteners to levelling-feet studs.

Components made of low-carbon steel

Types of low-carbon steel

There are different low-carbon steels with varying amounts of carbon. Below are examples of different types and their applications:

Type Industry Applications
Low-carbon structural steel Construction Buildings, bridges
Low-carbon sheet and strip steel Sheet metal work Automotive body panels, appliances and other uses that require thin, flat material
Low-carbon tubing and piping steel Construction, automotive, heavy equipment, oil and gas Mechanical tubes, pipes for fluid transport, and structural tubing
Low-carbon pressure vessel steel Heavy equipment, machinery manufacturing Boilers, pressure vessels and other uses where material must withstand high internal pressures
Low-carbon galvanised steel Construction, HVAC, automotive Roofing, automotive body panels, ductwork
High-strength low-alloy (HSLA) steel Construction Building frames, bridges, support structures


 

Grades of low-carbon steel

The most common standard organisation in the UK is:

  • BSI: The British Standards Institution, who have adopted ISO standards. On a technical sheet, they use ‘BS’ instead of their full initials. 
  • EN: The EN designation in BS (British Standard) grades of steel refers to the European standardisation system for steels. EN stands for "European Norm" and is a harmonised system of technical specifications for steel products across the European Union. Sometimes you’ll see a grade listed as BS EN. 

One of the most widely used standards is BS 970, which specifies a range of low-carbon steel grades. It covers the chemical composition of steel and the corresponding mechanical properties. The grades are designated by a four-digit number, which represents the chemical composition of the steel. The grades are designated by a four-digit number, which represents the chemical composition of the steel.

For example, let's take the BS 970 080M40 grade.

The first two digits ‘08’ represent the carbon content of the steel (0.8%). The next two characters ‘M40" represent the type of steel and its properties. In this case, ‘M’ stands for ‘manganese’ and ‘40’ indicates the minimum tensile strength of the steel in units of 1,000 pounds per square inch (ksi). So, the minimum tensile strength of BS 970 080M40 is 40 ksi.

Commonly used BS 970 grades and their typical applications include:

 

Grade Application
080M40 Shafts, axles
070M20 Bolts, nuts, & other fasteners
080A42 Gears, pinions, & other machine parts
080A15 Gears, pinions, & bushings
080M50 Crankshafts, couplings, spindles, high-strength bolts, gears & cams
150M19 Bushings, pins, & rollers
605M36 Gears, crankshafts, axles,high-strength bolts, nuts, & studs

Commonly used BS 970 grades of medium-carbon steel include:

Grade Application
080M30 Gears, shafts, axles
080M40 Bolts, studs & gears
605M36 Crankshafts, connecting rods & bolts
722M24 Shafts, bolts & gears
080A42 Cutting tools, eg: saw blades & knives
735A50 Gears for heavy machinery & equipment, eg: mining equipment, construction machinery & heavy trucks
655M13 Gears for heavy machinery, connecting rods, fasteners & bolts

Some of the most commonly used BS 970 grades of high-carbon steel include the following:

Grade Application
080A67  Cutting tools, e.g. saw blades
817M40 Crankshafts, gears, shafts, & bolts
060A96 High-stress components, eg: springs
735H51 Bearings & bushings
826M40 Gears, shafts, & bolts 
070M55 Ploughs, chisels & hammers
735A51 Bushings, springs, cutting tools, e.g. dies & reamers

For a detailed information about stainless-steel grades, read our article: Understanding stainless steel grades

Properties of low-carbon steel

Each grade has slightly different properties, although the melting point of low-carbon steel is about the same. That said, we can still give a range of values to give you an idea of this material’s overall properties.

Property Value
Density 2.85 – 8.08 g/cc
Tensile Strength, Yield 140 – 2400 MPa
Fracture Toughness 33.0 – 115 MPa-m½
Shear Modulus 70.0 - 80.0 GPa 
Melting Point 1430°C
Thermal Conductivity 25.3 – 93.0 W/m-K

 

Carbon steel flanges

What is medium-carbon steel?

Medium-carbon steel has a carbon content typically ranging between 0.3% and 0.6%. This category of steel offers a balance between the ductility and formability of low-carbon steel and the strength and hardness of high-carbon steel.

Medium-carbon steels are stronger and harder than low-carbon steels. This is due to their increased carbon content, but it also means they’re less ductile and more difficult to form and weld. They often require heat treatment, such as quenching and tempering, to achieve desired mechanical properties. This is possible with its manganese content, which ranges between 0.30% to 0.60%.

Concealed hinge

What are the uses of medium carbon steel?

Medium-carbon steels are commonly used in applications where higher strength and toughness are needed, as shown in the table below. It’s also used to make small components, such as concealed hinges.

Types of medium-carbon steel

Common types of medium-carbon steel and their applications include:

Type Industry Application
Medium-carbon structural steel Construction, Manufacturing Buildings, bridges, heavy-duty equipment
Medium-carbon sheet and strip steel Sheet metal work Machinery parts, Automotive parts
Medium-carbon tubing and piping steel Construction, automotive, heavy equipment Mechanical tubes, pipes for fluid
Medium-carbon pressure vessel steel Oil and gas, food and beverage, pharmaceutical Pressure vessels
Medium-carbon alloy steel Automotive, Heavy machinery Gears, shafts, axles, connecting rods
Medium-carbon quenched and tempered steel Automotive, Construction, Heavy machinery Gears, axles, transmissions, crane booms, excavation arms

 

Grades of medium-carbon steel

Products made from medium-carbon steel adhere to specific standards. Within those standards are grades. Commonly used grades of medium-carbon steel – and the standard they fall under – include:
 

Standard Grade Application
SAE J403 1045 Gears, shafts, machine parts
SAE J404 4140 Gears, axles, aircraft landing gears, and drilling equipment
ASTM A29 1045 Axles, bolts, studs, and other machinery parts
ASTM A576 1045 Bolts, studs, couplings, bushings, shafts and gears
ASTM A29 4140 Gears, axles, and shafts
ASTM A434 Class BD (AISI/SAE 4140) Bolts and other fasteners, connecting rods, gears and shafts
ASTM A829 4140 Gears, axles, and drilling equipment

 

Properties of medium-carbon steel

Each grade has its own properties that distinguishes it from other medium-carbon steel grades. The table below gives you a range of values for medium-carbon-steel properties.

Property Value
Density 7.75 - 7.89 g/cc 
Tensile Strength, Yield 245 - 1740 MPa
Fracture Toughness 80.9 – 143 MPa-m½
Shear Modulus 72.0 - 82.0 GPa
Melting Point 1425-1540°C
Thermal Conductivity 21.9 - 52.0 W/m-K

 

Carbon steel rods

What is high-carbon steel?

High-carbon steel contains a carbon content ranging between 0.60% – 1.5%. It’s the most corrosion resistant of the steels due to its high amount of carbon. This increased carbon significantly enhances the steel's hardness, tensile strength, and wear resistance. In turn, that makes it suitable for applications that demand high strength and wear resistance.

However, the higher carbon content also makes these steels more brittle and less ductile, which makes it more susceptible to cracking under certain conditions. High-carbon steel is also more challenging to weld than lower-carbon-content steels, due to the risk of cracking and brittleness in the heat-affected zone.

What are the uses of high-carbon steel?

High-carbon-steel uses include anything needing wear resistance and durability, as shown in the table below. A note about plain high-carbon steel, which is often used to mean high-carbon steel. They are different. Plain high-carbon steel consists mostly of carbon and iron, without any significant amounts of alloying elements.

High-carbon steel is often used to manufacture springs:

Types of high-carbon steel

High-carbon steel types, and their applications, include:

Type Industry Application
Plain high-carbon steel Manufacturing, automotive, construction Springs, knives, cutting tools, brake components
High-carbon tool steel Manufacturing, metalworking, woodworking Cutting tools, punches, dies, injection moulding tools, extrusion dies, router bits
High-carbon bearing steel Industrial machinery, automotive, aerospace Ball and roller bearings for engines; also, transmissions, wheels, heavy machinery, gearboxes, pumps
High-carbon spring steel Electronics, automotive, manufacturing Leaf springs, coil springs, machinery, springs for electronic devices

 

Grades of high-carbon steel

Grades of all carbon steels are subsets of specific standards. Some of the most commonly used grades of high-carbon steel include the following:

Standard Grade Application
ASTM A29/A29M AISI/SAE 1060 Springs, gears, axles, heavy-duty machinery components
ASTM A29/A29M AISI/SAE 1065 Springs, cutting tools, industrial knives and blades
ASTM A29/A29M AISI/SAE 1070 Springs, automotive suspension components, agricultural machinery parts
ASTM A29/A29M AISI/SAE 1080 Heavy-duty springs, automotive components, heavy machinery parts
ASTM A295 AISI/SAE 52100 Bearing steel used in the manufacture of ball and roller bearings
ASTM A600 AISI/SAE M2 High-speed tool steel used for cutting tools, drills, and taps
ASTM A686 AISI/SAE W2 Water-hardening tool steel used for cutting tools, dies, punches, and woodworking tools

 

Properties of high-carbon steel

Because standards and grades vary between each other, there is no one value for the properties of high-carbon steel. Below is a broad range of what you can expect.

Property Value
Density 0.451 – 8.26 g/cc
Tensile Strength, Yield 245 – 1740 MPa
Fracture Toughness 13.2 – 165 MPa-m½
Shear Modulus 78.0 – 82.7 GPa
Melting Point 1540 – 1590°C
Thermal Conductivity 19.0 – 52.0 W/m-K


 

The differences between low, medium and high-carbon steel

The essential difference is in the steels’ carbon content, which gives each different characteristics.

  Low-carbon steel Medium-carbon steel High-carbon steel
Carbon Content 0.05% to 0.32% 0.30% to 0.60% 0.60% to 1.5%
Characteristics Ductile
Malleable
Tough
Easily joined and welded
Poor corrosion resistance
Stronger
Harder
Less ductile
Less malleability
Good corrosion resistance
Very strong
Very hard
Poor ductility
Poor malleability
Better corrosion resistance

 

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download. You can also request free samples to ensure the product you’ve chosen is exactly what you need. 

If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you. Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.