Pros and Cons of Glass-Filled Nylon
As with any material, glass-filled nylon has its advantages and disadvantages. Understanding the pros and cons can help in determining its suitability for specific projects or requirements. In this guide, we’ll explore the key benefits and drawbacks of glass-filled nylon, providing valuable insights to aid in your decision-making and material selection. We’ll cover:
Introduction: What is Glass-Filled Nylon?
Glass-filled nylon, also referred to as glass-reinforced nylon or nylon composite, is a type of thermoplastic material. It’s formed by blending nylon with glass fibres, resulting in a composite material that exhibits improved mechanical properties.
By incorporating glass fibres, the strength, stiffness, and heat and wear resistance of the nylon are enhanced, making it suitable for demanding applications that require high performance and durability. The precise composition may vary, but typically glass fibres are added in proportions ranging anywhere from 10% to 40% by weight.
Glass-filled nylon offers numerous advantages over unfilled nylon. It boasts superior tensile strength, wear resistance, and dimensional stability. The glass fibres act as reinforcements, evenly distributing stress throughout the material, thereby reducing the risk of deformation or failure when subjected to loads. Its increased stiffness makes it particularly well-suited for applications necessitating rigidity and structural integrity.
Let’s compare the physical properties of unreinforced nylon with the properties of glass-filled nylon. The lower figure below is for unreinforced nylon and the higher values are typical of 30% glass-filled nylon.
- Tensile Strength: 90 – 185 N/mm²
- Notched Impact Strength: 5.0 – 13 Kj/m²
- Thermal Coefficient of expansion: 90 – 20/70 x 10-6
- Max Continuous Use Temp: 150 – 185°C
- Density: 1.13 – 1.35/1.41 g/cm3
Overall, this is a high-performance engineering material that combines the desirable properties of nylon, such as heat resistance, with the added strength and rigidity provided by glass fibres.
Glass-filled nylon vs. polymer
Glass-filled nylon and polymer are not mutually exclusive terms. Glass-filled nylon is a specific type of polymer composite. In other words, glass-filled nylon 6 uses nylon 6 as its base polymer. It’s the same with glass-filled nylon 66 – nylon 6/6 is the base polymer.
Learn more about these base nylons in The Differences Between Nylon 6 and Nylon 6/6.
The addition of glass fibres into other polymers is also possible. For example, polybutylene terephthalate (PBT) is a thermoplastic engineering polymer typically used as an insulator in the electrical and electronics industries. Adding glass fibres to PBT enhances dimensional stability, which allows for more precise fits – this makes glass-filled PBT fasteners, such as the push-in rivet shown here, ideal when you’re dealing with tight tolerances.
Advantages of Glass-Filled Nylon
It offers a multitude of advantages that contribute to its widespread adoption in a range of industries. Here are the material’s key benefits:
- Enhanced Strength and Rigidity: Glass-filled nylon strength is attributed to glass fibres, which significantly enhances the strength, wear resistance, and rigidity of nylon.
- Dimensional Stability: The material demonstrates superior dimensional stability, meaning it maintains its shape and size even under varying temperature and moisture conditions.
- Excellent Chemical Resistance: Glass-filled nylon retains the excellent chemical resistance inherent in nylon. It can withstand exposure to various chemicals, including oils, fuels, solvents, and corrosive substances, making it suitable for applications in chemically demanding environments.
- Outstanding Thermal Properties: Glass-filled nylon possesses excellent thermal resistance, including a higher heat deflection temperature of an average 113°C compared to unfilled nylon. This quality allows it to maintain its structural integrity and mechanical properties at elevated temperatures.
- Cost-Effective Solution: This is a cost-effective alternative to metals and other high-performance materials. It provides a balance between performance and cost efficiency, making it an attractive choice for manufacturers looking to optimise their production expenses without compromising on quality.
- Ease of Processing: Glass-filled nylon injection moulding is very common. The material is highly processable. Glass-filled nylon density gives it good flow properties, which facilitate the production of complex shapes and intricate designs with high precision. Glass-filled nylon filament is also common in 3D printing.
You can learn more about the injection moulding process in our guide, What is Plastic Injection Moulding and How Does it Work?
Disadvantages of Glass-Filled Nylon
Glass-filled nylon, like any material, has certain disadvantages that should be taken into consideration. Here are several potential drawbacks associated with glass-filled nylon:
- Increased Cost: Glass-filled nylon tends to be more expensive compared to unfilled nylon or other standard plastics. The addition of glass fibres raises the material cost, which can impact the overall manufacturing expenses of components.
- Higher Abrasion: Glass-filled nylon tends to have higher abrasive properties due to the presence of glass fibres. This means that it can cause more wear and tear when in contact with other materials, such as metal components or mating surfaces.
- Increased brittleness: While the addition of glass fibres enhances the material's strength and stiffness, it can also make the material more brittle. The presence of glass fibres in glass-filled nylon can create stress concentration points, leading to a higher likelihood of brittle fracture.
It's important to note that these drawbacks are general considerations and may vary depending on the specific formulation, glass-fibre content, and application needs.
Applications of Glass-Filled Nylon
Components made of glass-filled nylon are common for applications that require higher strength than unfilled nylon. Examples include:
25% glass-filled nylon for heavier-duty applications, such as securing and positioning components within the battery pack of an electric vehicle. Helps maintain proper spacing between battery modules, circuit boards, and other components, ensuring structural integrity and electrical insulation.
Through-Hole Angled Arch Pull Handle
30% glass-filled nylon handle is ideal for commercial doors and industrial equipment and machinery, allowing operators to easily open doors, access control panels, or operate machinery.
30% glass-filled nylon locknut designed to lock a cord grip in place. Perfect for outdoor electrical enclosures and equipment, industrial machinery, and automation systems.
25% glass-filled nylon bracket can accommodate multiple optical fibre cables. Ideal for data centres, telecommunications infrastructure and IT installations.
You’ll also find glass-filled nylon glides for brackets and lifting feet. Ideal for use in furniture, automotive and construction. Ensures the safety and longevity of the mounted structure or equipment.
Conclusion: Is Glass-Filled Nylon the Right Choice for Your Project?
Ultimately, the suitability of this material for your project depends on how well it aligns with your specific needs and objectives. Conducting thorough testing, consulting with material suppliers, and considering the trade-offs between properties and cost will help you make an informed decision regarding the use of glass-filled nylon in your project.
Download free CADs and try before you buy
Free CADs are available for most solutions, which you can download. You can also request free samples to ensure the product you’ve chosen is exactly what you need.
If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.
Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.
Questions?
Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.