The Advantages of Vented Screws
What are vented screws? This guide explains everything you need to know about these critical fasteners. Also known as vacuum vented screws, they come in different types, just as conventional screws do. For example, you can get vented socket head screws. So the question is, what’s unique about vented screws? This guide answers that question and covers:
Introduction to Vented Screws
Vented screws are a specialised type of fastener designed with a unique feature that distinguishes them from conventional screws. They incorporate a hole drilled through the centre to allow for the release of gases and pressure, typically in vacuum applications.
A blind tapped hole inside a vacuum system leaves residual air space at the bottom that cannot be fully evacuated in the vacuum cycle when a bolt, screw, or other fastener is threaded into the hole. The screw itself is a helix with a large surface area also containing voids of trapped air. This produces virtual leaks.
Vented screws and fasteners ensure direct ventilation of these voids, allowing the trapped volumes of air within the threads and at the bottoms of the holes to be fully evacuated. This speeds pump down and helps improve system performance.
The Advantages of Vented Screws
The function of vented screws goes beyond traditional fastening. This seemingly simple modification helps eliminate virtual leaks from high vacuum (HV and UHV) systems, thereby improving pump-down times. Trapped gases at the bottom of a tapped hole are able to escape via the central vent down the middle of the screw.
They are at their most effective when used with vented washers, which promote the release of gases trapped under the head of the screw. Let’s take a closer look at the advantages vented screws offer.
Improved Pressure Equalisation
Pressure equalisation involves maintaining a balance or equilibrium between the pressure inside and outside a sealed enclosure. Vented screws are often used in devices or enclosures that need to remain sealed from the external environment. Their job is to ensure that there is no significant pressure differential between the two environments.
If pressure inside and outside the enclosure differs due to changes in temperature or altitude, vented screws with channels allow air or gases to pass through. By effectively preventing the build-up of internal pressure, vented screws contribute to the safety, reliability, and performance of the application. Their ability to regulate pressure variations makes them a valuable component in ensuring the longevity and functionality of sealed enclosures and systems.
Preventing Build-up of Internal Pressure
The build-up of internal pressure within a sealed enclosure, system, or component can occur due to various factors such as temperature changes, chemical reactions, or mechanical processes within the sealed space.
Excessive internal pressure can have negative consequences, including the potential for damage to the enclosure, system failure, or even safety hazards. It can lead to the distortion or rupture of the sealed container or system components. Preventing or managing the build-up of internal pressure is important to maintain the integrity of the system and ensure its safe and reliable operation. Vented screws are ideal for allowing controlled release of the trapped air, thereby preventing overpressure.
Enhanced Airflow and Ventilation
This use of vented screws focuses on promoting airflow and ventilation within a system, component, or enclosure. They allow for the circulation of fresh air while expelling stale or polluted air. When used strategically, they create channels through which air can pass, helping to dissipate heat generated by components, such as processors, power electronics, or engines. This cooling effect prevents overheating, which can lead to performance degradation or even component failure. By enhancing cooling, vented screws contribute to the reliability and efficiency of machinery and electronic devices.
Applications of Vented Screws
Applications extend across various industries and settings where pressure regulation, moisture control, and airflow management are essential. These specialised fasteners play a crucial role in maintaining the integrity and performance of equipment and systems, from industrial machinery to aerospace components. In this context, vented screws find diverse applications, contributing to safety, reliability, and the longevity of critical components and systems. Common applications – and why vented screws are used – include the following:
Food Processing
Vacuum chambers are used to lower pressure, which, in turn, affects the vapour pressure of liquids within materials. This alteration induces a phase change, transforming liquids into gases, a process pivotal in drying food products. By reducing pressure, moisture is efficiently removed from food, extending its shelf life and preserving its quality.
Example:
- Vacuum drying machines
Industrial Machinery and Equipment
When industrial machinery and equipment operate in sealed or controlled environments, pressure equalisation is crucial. Vented screws help prevent damage caused by pressure differentials. By allowing controlled airflow, these screws ensure that the internal and external pressures remain balanced. This is vital in preventing leaks, maintaining seals, and preserving the integrity of equipment components.
Examples:
- Semiconductor manufacturing, which typically utilises ultra high vacuum (UHV), is among the most demanding industrial environments from the standpoint of outgassing and particulate contamination. A particle as small as one micron in size can cause a short in a device costing.
- Vacuum coating equipment, used to deposit thin layers of materials onto surfaces in industries like optics, electronics, and automotive
- High and ultra-high vacuum systems in controlled environments
- HVAC systems
- Outdoor equipment and structures, including solar installations
Fibre Optics
By conducting manufacturing processes in a vacuum, optical devices can achieve heightened performance, reliability, and precision, ultimately enhancing their effectiveness in their applications. This practice reflects a growing trend in the industry, underlining the critical role that vacuum environments play in optical device manufacturing.
Examples:
- Lens coating
- Laser optics
- IR detectors
Electronics and Electrical Systems
Electronics generate heat during operation. This makes efficient heat dissipation crucial to preventing overheating and maintaining component longevity. By providing airflow channels, vented screws help in heat dissipation by facilitating air circulation within enclosures, contributing to safe operating temperatures.
Consider, too, that electronics and electrical enclosures are often sealed to protect sensitive components from environmental factors. However, changes in temperature and altitude can lead to pressure differentials within these enclosures. Vented screws allow for controlled pressure equalisation, preventing damage to seals, gaskets, and delicate electronic components.
Examples:
- Control panels and cabinets
- Data Centres
- Instrumentation
Automotive and Transportation
Vented screws are often used in automotive parts to equalise pressure and prevent moisture buildup in the engine and other critical systems. They’re even used in glove boxes.
Aerospace and Aviation
Vented screws are instrumental in maintaining pressure equilibrium within aircraft components. This is critical due to the wide range of altitudes that aircraft operate in. Vented screws prevent pressure discrepancies that could otherwise lead to structural damage, potential leaks, or compromised seals, ensuring the overall safety and integrity of the aircraft. As altitude increases, air pressure decreases. By carefully controlling the amount of air in a vacuum chamber, conditions at specific altitudes can be created, enabling high altitude simulation for testing products and materials to be used in the aerospace or aeronautics industries.
Examples:
- Avionics bays and systems
- Instrumentation and cockpit
- Access panels and doors
- Environmental control systems
Medical Field
Maintaining a pristine, contaminant-free environment is critical in research labs and in medical manufacturing. Live samples are worked on and medication manufactured in a vacuum to avoid contaminates. Vented screws can be used in medical devices to prevent contamination during sterilisation.
Examples:
- Diagnostic imaging equipment
- Patient monitoring devices
- Laboratory equipment and cleanrooms
- Respiratory and ventilation devices
Read about other crucial components used in patient care equipment.
Types of Vented Screws
Conventional screws come in different types. So do vented screws. For example, just as socket head screws are available, so are vented socket head screws. Here are common types of vented screws and their uses.
Vented Countersunk Machine Screws
- Hex drive for precision assembling
- Ideal when surface area’s space is limited
- Centre vent reduces virtual leakage from high vacuum systems
- 304 Stainless steel – good strength and excellent corrosion resistance
- Hex drive for precision assembling
- Ideal when surface area’s space is limited
- Made from ultrasonically cleaned austenitic 304 Stainless Steel – good strength and excellent corrosion resistance
- Hex head for durability and precise torque application
- Reduced risk of stripping
- Easy to install or remove, even in confined or hard-to-reach spaces
- 304 Stainless steel for strength and corrosion resistance
Vented Screws – Socket Button Head
- Hex drive for precision assembly and when surface area is limited
- Low-profile head minimises the risk of snagging on clothing or equipment
- 304 Stainless steel for strength and corrosion resistance
You’ll also find it helpful to check out What is the difference between metric and standard fasteners?
Vented Washers
Our range of stainless steel vented washers are used with all types of vented screws to improve the speed and performance of creating vacuums in vacuum chambers. These are commonly used for industrial machinery or automotive components.
Download free CADs and try before you buy
Free CADs are available for most solutions, which you can download. You can also request free samples to make sure you’ve chosen the right product for what you need.
If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.
Whatever your requirements, you can depend on fast dispatch. Request your free samples or download free CADs now.
Questions?
Email us at sales@essentracomponents.com or speak to one of our experts for further information on the ideal solution for your application 800-847-0486.