A guide to leveling feet

Lady fitting levelling feet to a server cabinet

Leveling feet are essential for stabilizing furniture, machinery, and equipment across various industries. Whether you're looking for furniture leveling feet, heavy-duty adjustable feet, or machine feet, the right choice ensures stability, height adjustment, and vibration reduction. Learn more about these versatile components and their applications. In this guide, we’ll cover:

What are leveling feet?

Leveling feet, sometimes called level feet, are adjustable components used to stabilize and level furniture, equipment, and machinery. They’re commonly made of metal, plastic, or rubber and can be threaded. They serve three main functions:

Raising an application: By simply adjusting the thread length, you can easily increase the height of furniture or machinery. This is especially useful when frequent height adjustments are needed to create ergonomic workstations or align equipment with other components.

Leveling uneven surfaces: Tilting feet are specifically designed to compensate for uneven floors or surfaces. This ensures stability and prevents wobbling, even on inclined planes.

Reducing vibrations and noise: By creating a gap between the object and the floor, adjustable feet can significantly reduce the transmission of vibrations and noise. Rubber mounts, in particular, are highly effective in damping vibrations.

Vibration is more than just an annoyance. It can damage your application. Learn more in the guide our experts have put together, understanding vibration isolation

View our range of leveling feet

Articulating vs. non-articulating leveling feet

Articulating and non-articulating leveling feet are distinct in their structure and performance, particularly regarding how they manage uneven surfaces.

Articulating leveling feet

  • Structure: Features a base that can pivot or swivel, allowing the pad to adjust its angle relative to the threaded stem.
  • Purpose: Designed to provide stability on sloped or uneven surfaces, the swiveling motion reduces strain on both the foot and the equipment it supports.
  • Applications: Commonly used with industrial machinery, workshop equipment, and furniture placed on irregular surfaces where precise leveling is required.

Non-articulating leveling feet

  • Structure: These have a rigid base that does not move or tilt, keeping it fixed in a perpendicular position to the stem.
  • Purpose: Ideal for flat, even floors, these feet offer a straightforward and stable solution without additional moving parts.
  • Applications: Suitable for office furniture, appliances, or any setup on consistently level surfaces.

Key differences

Articulating leveling feet excel in environments with uneven ground by providing flexibility and stability, while non-articulating feet are best for flat surfaces, offering a simple and robust solution. The choice between the two depends on the specific demands of the equipment and its surroundings.

Where leveling feet are used

Leveling feet are often used in:

  1. Furniture – To ensure tables, cabinets, or chairs are level, especially in places with uneven flooring
  2. Appliances and equipment – For items like washing machines, refrigerators, or industrial machinery, appliance leveling feet help prevent tipping and vibrations
  3. Machinery – To maintain stability and precision in machines, industrial leveling feet are often used. 

Types of adjustable leveling feet

Leveling feet are designed for specific applications and requirements, so choosing the right type is crucial for ensuring safety, functionality, and durability. 

Leveling feet_ Ess_1460x500px 1

Stud mount leveling feet – plastic rigid base

Stud mount leveling feet with rigid plastic or nylon bases are designed to stabilize uneven surfaces and level machine tools and electronic racks. They also serve as: 

  • Light-duty machine feet
  • Office furniture leveling feet
  • Cabinet leveling feet
Leveling feet_ Ess_1460x500px 3

They feature low-carbon steel studs with zinc-plated finishes and nickel-plated shells, ensuring durability and an attractive finish. Nylon, low-density polyethylene, and polypropylene bases provide smooth, non-abrasive surfaces that protect floors and offer shock absorption for added stability. 

Leveling feet_ Ess_1460x500px 2

Some of our leveling feet within this range includes an integral hexagonal nut for adjustment under load, while others prioritize an economic design for cost-effectiveness. These screw-in feet combine functionality and aesthetics, making them suitable for a variety of applications.

View our range of stud mount leveling feet – plastic rigid base

Leveling feet_ Ess_1460x500px 4

Stud mount leveling feet – plastic swivel base

Stud mount leveling feet, also called swivel adjustable screw feet or threaded adjustable feet, stabilize machinery on uneven surfaces. By attaching to threaded inserts at the machine's base, they allow independent height adjustments to ensure stability and prevent tilting. 

Options include: 

  • Heavy-duty leveling feet that swivel with a 20-degree tilt and 2000 lbs load capacity for heavy equipment
  • Polypropylene feet available with a 25-degree tilt for added flexibility
  • Low-profile polyethylene or non-articulating polypropylene feet for lighter applications 

All variants feature durable zinc-plated steel threaded inserts.

View our range of stud mount leveling feet – plastic swivel base

Leveling feet_ Ess_1460x500px 5

Vibration mounts – heavy duty

Heavy-duty screw-on vibration mounts are designed to absorb shock and minimize noise. while providing strong adhesion to the floor. They can be used as a leveling device or even a bumper in small equipment. These durable mounts are ideal for use as feet on machinery and conveyors, offering enhanced stability and vibration dampening to protect equipment and improve operational efficiency. Made of thermoplastic elastomer (TPE).

View our range of heavy-duty vibration mounts

Leveling feet_ Ess_1460x500px 6

Extra: rubber covers & non-slip pads

Rubber covers and non-slip pads are versatile accessories designed to enhance the functionality of diameter levelers or conveyors by providing extra friction. 

Leveling feet_ Ess_1460x500px 7

These durable rubber pads are capable of supporting heavy loads while preventing movement or slipping, ensuring equipment remains stable and secure during use. Options include plain base or nylon and steel bolt-down base designs.

View our rubber covers & non-slip pads

You can learn more about leveling feet and another solution for furniture legs in our guide, Leveling feet and glides: everything you need to know.

How to find the right leveling feet for your applications

The right adjustable feet will help you improve your application’s stability, durability, and performance. To choose wisely, consider these factors:

Weight capacity:
Ensure the feet can support the maximum load, including the weight of the equipment and any additional stress.

Surface conditions:
For uneven or sloped surfaces, opt for adjustable or articulating feet. For smooth surfaces, non-slip pads or rubber-based feet can give you better stability.

Material compatibility:    
Select materials that suit the environment and application. 

Height adjustment range:
Choose feet with sufficient thread length or integral adjustment features to accommodate necessary height variations. 

Vibration & noise control:
If noise and vibration reduction is a priority, consider rubber or vibration-isolation mounts.

Mounting options:
Select screw-on, bolt-down, or free-standing designs based on your equipment's specific mounting requirements.

Aesthetic considerations:
In some cases, the appearance of the feet may be important. Choose finishes like chrome or nickel plating for a polished look.

Materials

Use this table as a general guide to how the materials compare with each other when deciding which leveling foot to choose. 

Material Characteristics Applications
Low-carbon steel Strong, durable, & capable of handling heavy loads; often zinc-plated for corrosion resistance. Threaded leveling feet for machinery, furniture, & cabinets.
Nylon Lightweight, non-abrasive, and shock-absorbing; resistant to wear & certain chemicals. Bases for rigid & swivel leveling feet; ideal for indoor or light-duty applications, such as chairs, tables, office desks, & small cabinets.
Low-density polyethylene (LDPE) Smooth, lightweight, & impact-resistant; provides non-abrasive surfaces but less durable than nylon or polypropylene. Rigid leveling feet bases for light-duty applications or flooring protection.
Polypropylene (PP) Stronger & stiffer than LDPE; can handle moderate loads, with good chemical and fatigue resistance. Swivel and rigid leveling feet bases, offering greater flexibility and tilt capabilities.
Thermoplastic elastomer (TPE) Flexible, rubber-like material with excellent shock absorption & vibration-damping properties; good grip on floors. Heavy-duty vibration mounts for machinery or conveyors where noise & vibrations need reduction.
Rubber High friction, excellent load-bearing capacity, & slip resistance; absorbs vibrations effectively. Covers & non-slip pads for leveling feet or conveyors to prevent movement & improve stability.
Steel Strong & durable, with zinc plating to resist corrosion; provides secure connections & weight support. Threaded inserts & bolt-down bases for securing leveling feet & accessories.
Nickel-plated shells Corrosion-resistant & visually appealing with a polished, durable finish; adds a protective layer to components. Enhances the appearance & durability of leveling feet, often used in environments requiring aesthetics.

 

EssFeet_1680x462px_B_1.jpg

Key takeaways

Load support:
Low-carbon steel, TPE, and rubber are the excellent materials for heavy-duty applications. Steel is essential for structural integrity, while TPE and rubber provide vibration damping.

Surface protection:
Nylon, LDPE, and PP are ideal for applications where floor protection and non-abrasive properties are critical, with nylon offering higher strength and durability.

Aesthetic appeal:
Nickel-plated shells enhance the appearance of leveling feet while providing additional resistance to wear and corrosion.

Shock absorption:
TPE and rubber excel in minimizing vibrations and noise, making them ideal for equipment that requires stability in dynamic environments.

Chemical & corrosion resistance: 
PP, nylon, and nickel plating perform well in resisting chemicals and moisture, making them suitable for challenging environments.

Cost & weight:
LDPE and PP are lightweight and cost-effective, while steel, TPE, and nickel-plated components offer durability and functionality at a higher price point.

Industries

Leveling feet are used wherever stability, precise leveling, and vibration control are critical. Common industries include:

Industry Application examples Choose
Manufacturing & machinery Stabilize industrial machines, conveyors, & equipment, ensuring alignment & reducing vibrations Heavy-duty stud mount leveling feet
Swivel base feet
Vibration mounts
Electronics & technology Level server racks, laboratory equipment, & sensitive devices Stud mount leveling feet with nylon or polypropylene bases
Swivel base feet
 
Furniture Level office furniture, cabinets, & desks, providing height adjustments & preventing wobbling Light-duty stud mount leveling feet
Non-articulating adjustable feet
Consumer appliances Ensure stability & alignment of appliances like refrigerators, washing machines, & dishwashers on uneven floors     Adjustable feet with rubber or plastic bases
Stud mount leveling feet

 

Leveling feet aren’t perfect for every application. You might find that bumper feet better suit your purposes. Our experts explain what you need to know in our guide, The benefits of rubber bumper feet.

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download. You can also request free samples for some solutions to make sure you’ve chosen exactly what you need. If you’re not quite sure which leveling foot will work best for your application, our experts are always happy to advise you.

Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.com or speak to one of our experts for further information on the ideal solution for your application 800-847-0486.