Nylon 6 vs. nylon 6/6

Young mechanical engineer pulling open a machine by its handle

Nylon is an important material which is used in a range of industrial applications including automotive industry, electrical panels & cabinets, telecommunications equipment and consumer electronics.

View our range of nylon components

What material is nylon?

It’s a high-performing engineering plastic. Specifically, it’s a thermoplastic linear polyamide with many variants. The most common we see used in engineering applications are nylon 6 and nylon 6/6, also referred to as nylon 66 and nylon 6.6, or using the polyamide name, PA 6 and PA 66.

What's the difference between nylon 6 and nylon 6/6?

The difference between these two nylon materials is in the numbers, which signify the type and quantity of polymer chains in their chemical structure.

Polyamide structure

Nylon 6: Derived from one monomer, which is a molecule that can be bonded to other identical molecules to form polymers. For nylon 6, the monomer has six carbon atoms, hence the name nylon 6. The chemical formula of nylon is (C6H11NO)n.

Nylon 6/6: Made from two monomers. Each of these monomers has six carbon atoms, which is reflected in the name nylon 6/6. Its chemical formula is (C12H22N2O2)n.

Polyamide production requires the repeated joining of two groups to form an amide link. Amide is the organic compound containing the group C(O)NH2.

Nylon 6

Nylon 6

Nylon 6/6

Nylon 6/6

As you’d expect, nylon 6/6 is stiffer and usually more durable. However, they do share many of the same characteristics.

Nylon properties

Nylon uses are vast, including snap latch rivetsnylon hex nuts, flat washers, push rivetscable twist ties, door panel retaining clips and cable strain reliefs.

Polyamide advantages – and a few of their disadvantages – include:

  • High mechanical strength
  • High toughness, stiffness and hardness
  • Good fatigue resistance
  • Good impact resistance
  • Excellent wear resistance
  • Good electrical insulating properties
  • No resistance to UV rays
  • Lightweight; sometimes used in applications in place of metals
  • Excellent fuel and oil resistance
  • Attacked by strong mineral acids and absorbs polar solvents
  • High water absorption

Nylons and UV rays

Nylons are not UV resistant, although you can add stabilizers to give them almost any effect you desire. This is why nylon temperature range can vary. On their own, nylon 6/6 is the more sensitive, though nylon 6 is still vulnerable without stabilizers.

UV light weakens nylon through interaction with the chemical structure’s pi electrons, specifically double bonds and aromatic groups. Nylon 6, for example, absorbs UV light in its amide bonds. Polymers that lack pi electrons, such as polyethylene, can stand up better to UV rays.

Mini Snap Together Rivets - Line Drawing

UV rays affect all materials, not just nylons. But with stabilizers, nylon can perform extremely well outdoors. For example, usage of nylon includes these mini snap rivets made of nylon 6/6 with a UL94 V-2 flammability rating ideal for outdoor applications:

Electrical components inside a laptop

At a glance: Nylon 6 and nylon 6/6 material properties

It comes down to a lot of little things. While both nylon plastics are cost effective, Nylon 6 typically costs around 30% less. Here’s a closer look at the differences:

Attributes Nylon 6 Nylon 6/6
Machinability – low tool wear & surface finish Good Better
Mold shrinkage Lower Greater
Water absorption rate Higher Lower
Impact strength Izod: cm-N/cm of notch: 160 Izod: cm-N/cm of notch: 160
Tensile strength 6.2 x 104 kPa (Good) 8.2 x 104 kPa (Better)
Crystalline melting point 437°F / 225°C 509°F / 265°C
Density 1.15 g/ml 1.2 g/ml
Typical molding shrinkage ratio 1.2% 1.5%

 

How nylon 6 and nylon 6/6 compare in manufacturing

Both have very good flow for easy processing.

As shown in the table, nylon 6 processes at a lower temperature, while nylon 6/6 has a higher melting point. This presents more challenges for processing nylon 6/6. When nylon 6/6 is exposed to ambient air temperatures and begins to solidify, mold shrinkage occurs and shapes can change. However, you can get around this by increasing the dimensions of your extrusion dies and injection molds. Nylon 6 is another matter, which processes much easier. Because its mold shrinkage is lower than nylon 6/6’s, you get more reliable final part dimensions.

Another issue with processing nylon materials is moisture and water absorption. In this regard, nylon 6 absorbs more than nylon 6/6, but both materials will need to be dried before being molded. The reason: nylon absorbs moisture from the air. Failure to dry the material will lead to splays and marks on part surfaces. Keep in mind that oxidation occurs due to heat and water, so if you skip the drying process, you’re also looking at compromised mechanical properties as a result of material degradation.

Injection molding and drying nylons

If you over-dry nylons, the finished part could come out brittle. Follow these guidelines for both nylon 6 and nylon 6/6:

If moisture content is greater than 0.2%:

Method of drying Temperature Duration
Hot air oven 176° F (80° C) 16 hours

If nylon has been exposed to air for longer than 8 hours:

Method of drying Temperature Duration
Vacuum 221° F (105° C) 8 hours
Man using an office printer with digital display

What is glass-filled nylon?

You can add powdered glass to nylon resins, which will increase:

  • Tensile strength
  • Compression strength
  • Stiffness

This process will also give you a lower thermal expansion coefficient than unreinforced nylon. Remember, nylon absorbs moisture. That, in turn, causes the material to expand. Adding glass fibers offsets this problem, increasing stability when the nylon is exposed to temperature changes.

Find out more about glass-filled nylon in our guide, Pros and Cons of Glass-Filled Nylon.

In the first table we showed you, nylon 6’s typical molding shrinkage ratio is 1.2%, and nylon 6/6, 1.5%. By adding 30% glass fibers to nylon 6, this can be reduced to 0.4%. Add 33% to nylon 6/6, and you’re looking at 0.5%.

All that aside, when you need to enhance the strength of nylon, glass filled, or GF nylon, is ideal. In fact, by using glass as an additive, you can strengthen your nylon by up to 70% more than untreated nylon.

An example of a GF nylon solution is Essentra’s hexagonal standoff, which is 25% glass filled, nylon 6:

Hexagonal Standoff - Line Drawing

Nylon applications

Nylon’s characteristics make it a popular material across all industries and applications. Here are some examples of products made from nylon plastic.

View our range of nylon components

Nylon 6/6:

Nylon cable ties

 

Nylon cable ties

General purpose, across all industries.

Adjustable cable clamps

 

Adjustable cable clamps

Can easily open to make routing changes. A wire cable clamp is used in everything from electrical cable enclosures to PCBs.

Plastic push rivets

 

Plastic push rivets

Nylon rivets are used in everything from appliances to computers and panels.

Cable twist ties

 

Cable twist ties

From automotive to office machinery and equipment, cable management twist ties come in different mounting types.

Nylon 6:

Panel catches

 

Panel catches

Keeps thick doors and panels securely closed by mounting through diameter holes.

Industrial handles

 

Industrial handles

Industrial door pull handles made of nylon 6 are ideal for machine covers.

Card guides

 

Card guides

Mount your PCB in tight spaces while giving them a level of protection.

Snap-latch rivets

 

Snap-latch rivets

Ideal for applications that require maintenance work. Available in easy-grip or mini-grip designs for different panel holes and thicknesses.

Alternatives to nylon

Nylons aren’t ideal for every application, of course. For instance, nylon fasteners work great in many instances, but other plastics might suit your project better.

For help deciding, check out our guides, How to choose nylon screws and A guide to nylon fasteners

You may also consider acetal instead of nylon for your application. Both are commonly used to make small components for industries ranging from automotive to electronics. Find out more in our guide, Differences between nylon and acetal.

You can also learn more about plastics with our Ultimate Caps and Plugs Guide.

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download. You can also request free samples to make sure you’ve chosen the right product for what you need. 

If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.

Whatever your requirements, you can depend on fast dispatch. Request your free samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.com or speak to one of our experts for further information on the ideal solution for your application 800-847-0486.

View our range of nylon components