304 vs. 316 stainless steel: what’s the difference?

Stainless steel pipes in food processing

Both are part of the austenitic family of stainless steels, sharing a similar chemical composition. While this means many of their attributes are the same, there’s also a distinct difference. In this guide, we’ll look at the content of those two stainless steel grades and their unique properties – and how both express themselves in terms of characteristics: 304 vs. 316 stainless steel strength. 304 vs. 316 stainless steel uses. We’ll cover:

What is 304 stainless steel?

304 stainless steel alloys include a minimum of 18% chromium and 8% – 10.5% nickel with a maximum of 0.08% carbon. 

As a general rule of thumb, austenitic stainless steels contain significant amounts of chromium and nickel, and that’s really what gives this family of steels their excellent corrosion resistance. Chromium provides a protective oxide layer. It does something else, too, with the addition of nickel – they enhance toughness and ductility, making the steel easy to work with. As austenitic stainless steel contains less iron than say, a ferritic stainless steel, this stainless-steel family is typically non-magnetic, though some have slight magnetic characteristics. 

Specifically, 304 stainless steel is the most widely used of all stainless steels, which comes down to its properties. 

You can learn more about stainless steel in our guide, Understanding stainless-steel grades

What is 304 stainless steel used for?

Some of its common industrial applications include:

Industry Typical applications Why
Food processing equipment Tanks, pipes & containers Resistance to corrosion, easy to clean
Consumer appliances Sinks, refrigerators, dishwashers Durability, resistance to corrosion, aesthetic appeal
Automotive Exhaust systems, trim & grilles Resistance to corrosion, aesthetic appeal
Medical equipment Surgical instruments, dental instruments & implants Biocompatibility, resistance to corrosion & withstands high-temperature cleaning processes
Chemical processing  equipment Reactors, tanks & pipelines Resistance to corrosion, stands up to a range of chemicals
Aerospace components Aircraft structures, engines High strength-to-weight ratio, resistance to corrosion, thermal stability

 

304 stainless steel is also used in different types of small components. Just some examples include:

What is 316 stainless steel?

Grade 316 is another austenitic stainless steel. As part of the 300 series of austenitic stainless steel, it also contains nickel, just as 304 does. Where 304 stainless steel alloys have a minimum of 18% chromium, 316 stainless steel has less with 16%. The nickel content in 316 is also higher, at 10%. 

You would think this would give 304 stainless steel a higher resistance to corrosion, but 316 contains 2% molybdenum. The molybdenum helps resist corrosion caused by chlorides, such as sea water and de-icing salts. It also gives 316 greater resistance to chemical attacks. 

While each offers excellent corrosion resistance, 316 stainless steel’s is actually higher than grade 304 stainless steel. Grade 316 often exhibits better strength at high temperatures, although both have excellent heat resistance.

Grade 304 vs. 316 stainless steel appearance is impossible to judge by the naked eye – they look the same, except when it comes to cost. Expect to pay more for 316, which is due to the higher nickel content and addition of molybdenum. 

What is 316 stainless steel used for?

304 vs. 316 stainless steel uses often comes down to budget. Grade 316 can be used for the same applications as 304 – as you’ll see below – but 304 can’t always be used instead of 316. Here are just some of the industries and applications where 316 is put to work. 

Industry Typical applications Why
Food processing equipment Tanks, pipes & containers Non-reactive – does not impart any unwanted flavours or odours to food & easy to clean
Oil and gas Pipelines, valves & fittings Resistance to corrosive fluids and gases
Energy/power generation Turbine blades High-temperature strength & corrosion resistant
Medical equipment Surgical instruments, dental instruments & implants Biocompatibility, corrosion resistant & withstands high-temperature cleaning processes
Chemical processing equipment Production of organic acids, storage tanks & reactors Molybdenum enhances corrosion resistance, high-temperature strength 
Marine Boat fittings & seawater piping Highly corrosion resistant in marine environments

 

316 stainless steel is considered marine grade, but it’s not resistant to warmer sea water (304, even less so), which can cause chloride pitting. Still, its characteristics make it popular for use in small components too. Examples of common applications include:

Stainless steel pipework

304 vs. 316 stainless steel properties

As austenitic materials, their properties are similar. In the case of 304 vs. 316 stainless steel properties, they’re identical or nearly the same, which comes down to their similar chemical composition. For instance, their densities are often the same, despite the addition of molybdenum to 316. However, molybdenum has a relatively low atomic weight, so it doesn’t have much of an impact on density. 

Properties of 304 and 316 stainless steel

304 vs. 316 stainless steel: a comparison

Let’s compare their content. Again, note that they share much of the same content – except for molybdenum. Grade 316 also has more nickel, while 304 has more chromium. 

Element 304 stainless steel % 316 stainless steel %
Carbon 0.07 0.07
Chromium 18.0 – 19.5 16.5 – 18.5
Nickel 8.0 – 10.5 10.0 – 13.0
Silicon 1.00 1.00
Manganese 2.00 2.00
Phosphorous 0.045 0.045
Sulphur 0.015 0.015
Nitrogen 0.10 0.10
Molybdenum - 2.0 – 2.5

 

304 vs. 316 stainless steel strength

When it comes to mechanical strength, 316 stainless steel is generally considered stronger than 304. Again, this is attributed to 316’s molybdenum content. As a result, 316 stainless steel generally has better mechanical properties. The yield and tensile strength of each vary, depending on the manufacturing process and conditions involved – but in general, the tensile strength of 316 stainless steel is higher than that of 304 stainless steel.

Choosing between 304 and 316 stainless steel comes down to your application and its specific requirements for oxidation resistance, mechanical strength, and ultimately, cost. For example, if your application won’t be in a highly corrosive environment, go with grade 304. It’s still extremely resistant to corrosion, but it also costs less. At the same time, using 304 in applications that are better suited for 316 stainless steel can end up costing you more in the long run. 

To understand the Rockwell B hardness test below, see our guide, What’s shore hardness and why should you care?

Mechanical properties 304 stainless steel 316 stainless steel
Ultimate Tensile Strength 505 MPa 550 MPa
Tensile Yield Strength 215 MPa 240 MPa
Hardness (Rockwell B) 70 80
Elongation at break 70% 60%

 

304 vs. 316 stainless steel differences

In summary, these are the primary characteristics of each stainless steel:

Characteristics 304 stainless steel 316 stainless steel
Corrosion resistance Excellent Even better
Magnetic No No
Weldability High Good
Hardens during cold forming Yes Yes
Formability Very good Good
Machinability (annealed) Fair, but better than 316 Fair
Resists elevated temperatures High High
Maximum intermittent service temperature 850°C 850°C


 

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download. You can also request free samples to ensure the product you’ve chosen is exactly what you need. 

If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you. Whatever your requirements, you can depend on fast despatch. Request your free samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.