Lead Screws vs Ball Screws: What's the Difference?

Lead screws and ball screws

The discussion over ball screw vs lead screw is becoming increasingly debated as designers and engineers work to achieve ever-higher accuracy and dependability. Lead screws and Ball screws can make a significant impact on the performance, efficiency, and overall functionality of a linear motion system. 

These fundamental components play a pivotal role in transforming rotational motion into linear motion, a process essential for countless applications ranging from 3D printing and CNC machines to robotics.

Prior to deciding between a lead screw mechanism or a ball screw for your application, it’s crucial to understand the unique characteristics of each and determine how well they align with your specific requirements. In this article, we’ll look at both and give you an understanding of how each component work, covering:

What is a ball screw?

A ball screw is a mechanical component designed to convert rotational motion into linear motion with enhanced precision and efficiency. 

Ball screw

Consisting of a screw shaft and a nut containing recirculating ball bearings, the ball screw operates on the principle of rolling contact rather than sliding friction.

Ball screw diagram

These small ball bearings move along the thread of the shaft as the ball screw rotated. This provides smooth, low-friction movement. They are used to convey forces to a moving or stationary load with exceptional precision, accuracy, and repeatability. Ball screws find extensive applications in various industries such as manufacturing, robotics, aerospace, and automation. 

Note: You must not remove the ball actuator from the sleeve, as the balls will come loose, and the nut will become unusable.

Take a look at our range of ball screws.

What is a lead screw?

When ball screws may not run well in "dirty" or other corrosive situations, lead screws may be more beneficial. They can also outperform ball screws in vertical running applications and create less noise..

Lead screw linear actuators have nut threads and a moving screw shaft; there are no ball bearings in between. Higher energy losses due to friction are produced when the nut and screw shaft move directly against one another across a wide contact area.

Lead screw diagram

In addition to being less expensive than ball screws, high precision lead screws are produced to tighter tolerances than normal lead screws, despite the fact that they’re  generally regarded as less accurate.

Lead screw

Take a look at our range of lead screws.

To expand their benefits and range of applications, ball and lead screws are combined with linear bushings or guideways, improving their performance. Choosing the right linear bushing is essential when it comes to linear motion systems. 

To navigate your way around these components check out our guide on How To Select the Right Linear Bushings for Your Application.

What are the key differences between ball screws and lead screws?

Examine the chart below to understand the differences between ball screws and being screw lead. This will help you decide which is best for your application. Consider your specific requirements and compare the characteristics to find the best fit:

Screw Type Advantages Disadvantages
Ball Screws Low friction
Needs less torque
Creates less heat
Lifespan
Exceptional precision
Higher load capacity
More expensive
Creates more noise
Ball bearings more susceptible to obstructions
Can require braking system
Requires lubrication for ideal operation
Complex design
Lead Screws Cost effective
Self-locking, no braking system required
Suitable for vertical applications
Simple design
Needs more torque
Shorter lifespan
Creates more friction and heat
Lower precision
Natural backlash
Lower load capacity

 

Benefits of using lead & ball screws

The choice between a screw drive actuator, such as ball screws or lead screws, hinges on the specific needs of your application. If precision, high-load capacity, and efficiency are top priorities, ball screws may be the preferred option. However, for projects with budget constraints, simpler requirements, or where the environment could be corrosive, lead screws offer a practical alternative without compromising functionality.

Applications & Uses

Below shows you the most suitable screw lead applications:

Application Lead Screws Ball Screws
Manufacturing (Conveyors, assembly lines)
CNC Machining
Robotics (Robotic equipment)
Automotive (Adjustable seats and sunroof mechanisms)  
Medical (Imaging devices and equipment)    
Aerospace (Aircraft components)
Printing and Packaging (Packaging machinery)  
3D Printing (Machines that use movement systems)  

 

Whether in manufacturing or automated systems, the versatility of these screw lead components allow engineers to tailor motion systems with a keen eye on efficiency, precision, and reliability. 

Lead screws are often chosen for applications that require manual adjustments. As an example, when integrated with shaft clamp accessories, users can easily and quickly secure or release the lead screw, allowing for rapid adjustments or repositioning without the need for specialised tools. 

Ball screws, known for their precision in linear motion, can also benefit from shaft clamps. In applications requiring precise positioning or adjustments, with rapid securing of the ball screw.

The combination of lead screws, ball screws, linear shafts and bushings and accessories create a wide range of suitable applications, as long as the specific requirements matches the characteristics of each type of component.

Sizes & Materials

When it comes to screws in linear motion systems, it’s crucial to select other components that compliment them well – such as linear rails or shafts. The components need to be compatible and can increase performance, durability and efficiency.

For more information, don’t miss our guide, How to Select the Ideal Linear Shaft for Your Application.

Lead screws can be composed of steel, or corrosion resistant stainless steel, whereas ball screws are generally made of steel. Leadscrew nuts are commonly made from steel or bronze, have self-lubricating properties, and therefore offer low friction performance when used. 

Screws crafted from steel alloys, such as carbon steel or stainless steel for corrosion resistance, have a balance of strength and cost-effectiveness. Both these material choices offer performance and durability when it comes to applications of linear shaft systems.

To help you learn more, our experts have put together the guide Choosing the Right Captive Screw.

Download free CADs and try before you buy

Free CADs are available for most solutions, which you can download. You can also request free samples (some exclusions apply) to ensure the product you’ve chosen is exactly what you need. 

If you’re not quite sure which solution will work best for your application, our experts are always happy to advise you.

Request your samples or download free CADs now.

Questions?

Email us at sales@essentracomponents.co.uk or speak to one of our experts for further information on the ideal solution for your application 0345 528 0474.